Cat GRADE with ASSIST Makes Accurate Grading Fast & Easy

For Release in Europe: April 2016
Release Number: 117PR16

Cat® GRADE with ASSIST makes the Cat 323 hydraulic excavator more efficient and productive. This system is the first operator ASSIST feature with semi-autonomous grade control available on Cat excavators, and it automates grade adjustments that are typically achieved by the operator using manual controls. Operators at all experience levels can reach target grade as much as 45 percent faster than traditional grading.

Optimized for Cat excavators, this new technology is easy to use from the start. Integration with the familiar Cat GRADE system, display, and joysticks enables the operator to easily create simple 2D designs in the cab, press the auto button, and get to work. Operators can take advantage of the guidance features built into the base system without the need for data transfer infrastructure. For example, grade indication and audible alerts function while using ASSIST technology to perform precision work—without the need for infrastructure.

Integration with the machine and hydraulics delivers full power to the cutting edge with precise control throughout the cut, enabling the operator to create fast, accurate grades with less effort. System flexibility enables customers who work with complex grade plans to add Cat AccuGrade™ for additional 3D capability.

Automatic assistance and protection features

ASSIST technology goes to work when the cutting edge gets within 10 cm of target by locking on grade and automatically adjusting boom up/down and bucket in/out movements. The operator simply controls stick speed using a single lever, which significantly reduces manual inputs. The system also automates bucket movements to maintain a constant bucket angle, which is operator adjustable to match cutting angle to digging conditions and can be automatically recalled for next pass. To eliminate the chance of overcutting, a grade protection feature prevents the cutting edge from penetrating below grade, saving contractors the time and cost of rework, additional fuel, grade checking, labor hours and fill material.

In addition to helping customers speed grading, PROTECT features safeguard the operator and machine when working near obstacles and around utility hazards. Ceiling and Floor PROTECT prevent any part of the boom, stick, or bucket from going above or below a pre-set elevation, enabling the machine to excavate in areas with low ceiling heights such as indoors and under overpasses and near above- and below-ground utilities. Operators can quickly disable AUTO control with an override trigger at their fingertips.

Features and functions

Intelligent control and protection features assist contractors in getting more work done. Functions include:

  • GRADE with ASSIST – automatically adjusts boom up/down and bucket in/out to maintain constant grade.
  • Operator ASSIST – operator controls stick speed using single lever with one hand.
  • Bucket Angle ASSIST– automates adjustments to maintain a constant bucket angle.
  • Grade PROTECT – prevents the cutting edge from penetrating below grade.
  • Ceiling PROTECT + Floor PROTECT– prevents any part of the boom, stick, or bucket from going above or below a pre-set elevation.
  • Operator OVERRIDE – enables the operator to override AUTO functionality.
  • 2D and 3D Control – works with existing 2D grade indication system; can be upgraded to AccuGrade for 3D positioning and elevation guidance.

                                                                                                                        # # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “AccuGrade”, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2016 Caterpillar All Rights Reserved 

Alt Alt