Caterpillar Exclusive Three-Dimensional Screed Plate System
Caterpillar Exclusive Three-Dimensional Screed Plate System

Caterpillar Exclusive Three-Dimensional Screed Plate System

 

For Release in North America: March 2023
Release Number: 112PR23

As previously announced, Caterpillar Inc. has entered into an agreement with construction solutions supplier, Axenox, Inc., to acquire the intellectual properties of two of the company’s asphalt paving screed products. Under the agreement, three-dimensional screed plates and the modular screed plate fastening system will be available options exclusively for Cat® asphalt paving customers.

These new innovations are true market disrupters for the asphalt paving industry,” comments Nate Just, marketing manager for Cat Paving Products. “The innovative three-dimensional screed plate design improves mat density and smoothness as well as density at the joint to reduce compaction expense and improve the chances of achieving bonus. The modular fastening system reduces the time required to replace screed plates by more than 80% to lower costs and maximize paver uptime availability.”

Brothers Michael and Stuart Frost, long-time paving contractors and owners of Axenox®, invented the innovative screed system to improve paving efficiency and quality for their paving operations. “Basic screed design had never changed in our lifetime or our father’s, so my brother and I developed our own screed. We knew we had something special with this technology,” says Stuart Frost. Michael Frost adds, “We want to see this effect the industry in a positive way, just like it has for our paving operations. That’s why we chose Caterpillar and the second-to-none support offered by the Cat dealer network as the best way to carry out our vision.”

Increased density and smoothness

The Axenox® screed plate design is a significant departure from industry standard. Whereas traditional plates are flat, these plates utilize a three-dimensional, angular design. This added dimension delivers lateral compaction confinement to asphalt material. The kneading action helps aggregate to interlock more efficiently than with flat screeds, increasing mat and joint density along with improving mat smoothness.

Densities reaching 91% have been measured behind pavers equipped with the three-dimensional screed plates, so there is less of a chance for material shoving and cracking with the roller. These high densities can reduce the number of passes, lowering compaction cost. At the longitudinal joint, higher densities result in improved material containment during compaction to increase final density. Uniform mat temperatures gained by using the angular plates also help to reach specified densities more easily, helping contractors to meet bonus-level work.

The stiffer asphalt mat left behind the three-dimensional plates allow the breakdown roller to achieve higher densities before the mat reaches the tender zone. It produces a more stable unconfined edge that resists pushing and shoving by the breakdown roller, so consistent density readings are achieved across the entire mat width.

The three-dimensional cast plates are made with high strength chromium carbide, delivering high wear resistance and longer life in the field. Whereas traditional screed plates are run with an elevated front angle of attack, increasing wear, grooves at the front of these plates act as the angle of attack, so they run flat to wear more uniformly and reduce cost.

Fast changes 
A revolutionary new way to secure the plate to the screed, the modular fastening system reduces screed plate change time from days to less than four hours, minimizing replacement costs for the paving contractor. After a one-time installation of the insulated conductor plate, simple screed plate changes are completed using a unique lock-and-go system. This eliminates the time-consuming process of removing asphalt material from the screed to access the nuts and bolts holding the plates in place. Once normal screed set-up and adjustments are completed on the conductor plate, minimal adjustments are required on future screed plate changes.

Contact your Cat® Dealer for more information about the new three-dimensional screed system. 

 

Download the press release and images 

Download Now

 

 

of

Oxclaw® textured screed plates and Bullox® modular screed plate system will be available options exclusively for Cat® asphalt paving customers.

View Full Size Image
of

Oxclaw’s innovative three-dimensional textured screed provides lateral compaction confinement to asphalt material.

View Full Size Image
of

The Axenox® screed system will be exclusively available for Cat customers and supported by the extensive Cat dealer network.

View Full Size Image

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

# # #

 

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2023 Caterpillar All Rights Reserved 

 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Johanna Kelly: Kelly_Johanna_L@cat.com

Reader Requests
www.cat.com/requestCatinfo