Caterpillar Inc. is launching its next generation of Cat® Telehandlers. Released for retail and rental customers, the Cat TH0642, TH0842, TH1055 and TH1255 models replace the previous TL642, TL943, TL1055 and TL1255 machines.
IRVING, Texas, January 7, 2025―Caterpillar Inc. is launching its next generation of Cat® Telehandlers. Released for retail and rental customers, the Cat TH0642, TH0842, TH1055 and TH1255 models replace the previous TL642, TL943, TL1055 and TL1255 machines.
Kevin Coleman
Senior Product Consultant
Cat Telehandlers
The new Cat Telehandlers are powered by the Cat C3.6TA (turbocharged and aftercooled) engine that meets U.S. EPA Tier 4 Final/EU Stage V emissions standards. The 74 hp (55 kW) engine includes a zero-service diesel particulate filter (DPF) and does not require diesel exhaust fluid (DEF). A 115 hp (86 kW) option for the TH0842, TH1055, and TH1255 models also uses selective catalytic reduction (SCR) technology.
The telehandlers offer three operator station options: open canopy, enclosed cab with heat and enclosed cab with heat and air conditioning. The redesigned interior features an ergonomic control layout, standard tilt steering column, and a new full color LCD monitor that provides machine information in a choice of four languages – English, French, Spanish or Portuguese. The monitor also shows the standard rearview camera feed when in reverse and depressing the camera soft key enables continuous viewing of the camera image. Additional standard equipment includes the standard operator presence seat switch to prevent machine operation when the operator is not seated. The optional Load Stability Indication (LSI) system provides visual and audible alerts to the operator regarding forward machine stability while handling a load.
The pilot-controlled joystick ensures a smooth, predictable multi-function performance and feel of the boom extend/retract and lift/lower functions. Customers now have a choice of coupler interface; the IT or Standard TH. Smaller and lighter weight than the IT style coupler, the new Standard TH quick coupler offering delivers improved fork visibility and enhanced load capacity when used with the boom extended. The next generation Cat Telehandlers also feature standard auxiliary hydraulics to support hydraulically powered Cat attachments.
To assist with fuel economy and minimizing idle time, Cat Telehandlers are equipped with a configurable engine idle shutdown feature.
The monitor in the Cat Telehandlers features a standard multi-operator code security system, supporting up to 50 operator codes to protect against machine theft and unauthorized use at the jobsite.
The new TH models feature extended service intervals and a patent-pending service tool for quick inspection of chains and boom wear pads. The boom sections, mainframe, stabilizer frame and stabilizer legs are covered by a 5-year, 5,000-hour warranty.
Equipped with Product Link™ Elite standard telematics, the system provides critical machine operating information for fleet managers. Remote flash capability allows for software updates without a trip to the dealer’s shop, and remote troubleshooting provides real-time diagnostics, along with remote machine parameter and setting changes.
Caterpillar will display the next generation Cat Telehanders at World of Concrete 2025 in booth C6061.
Target availability for these next generation telehandlers is Q2 2025. More information on the new Cat Telehandlers can be found by contacting a Cat dealer or visiting cat.com.
Model |
TH0642 |
TH0842 |
TH1055 |
TH1255 |
Engine |
Cat® C3.6TA |
Cat® C3.6TA |
Cat® C3.6TA |
Cat® C3.6TA |
Gross power ISO 14396, hp (kW) |
74 (55) |
74 (55) |
74 (55) |
74 (55) |
Gross power option ISO 14396, hp (kW) |
N/A |
115 (86) |
115 (86) |
115 (86) |
Operating weight, lb. (kg) |
21,647 (9819) |
23,366 (10 599) |
29,838 (13 534) |
31,238 (14 169) |
Maximum lift height, ft (m) |
42.1 (12.8) |
42.1 (12.8) |
54.6 (16.6) |
54.6 (16.6) |
Maximum forward reach, ft (m) |
27.6 (8.4) |
27.6 (8.4) |
41 (12.5) |
41 (12.5) |
Travel speed forward, mph (kph) |
19 (30) |
20 (31) |
18 (30) |
18 (30) |
Travel speed reverse, mph (kph) |
14 (22) |
14 (22) |
13 (22) |
13 (22) |
Auxiliary hydraulic pressure, psi (bar) |
4,061 (280) |
4,061 (280) |
4,061 (280) |
4,061 (280) |
Auxiliary hydraulic flow, gpm (lpm) |
14.5 (55) |
14.5 (55) |
14.5 (55) |
14.5 (55) |
# # #
About Caterpillar:
With 2023 sales and revenues of $67.1 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For nearly 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels at caterpillar.com/en/news/social-media.html.
Note to Editors: Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, VisionLink, MineStar, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
Caterpillar Inc. is announcing the new Cat® D8 dozer with advanced technology designed to provide faster more accurate results.
Learn MoreCaterpillar Inc. will launch its Centennial Celebration during CES 2025, providing visitors the opportunity to reflect on the company’s global impact over the last century and envision what’s in store for the future.
Learn MoreCaterpillar is announcing Cat® Command for Loading is expanding to all medium wheel loaders, excluding the GC models.
Learn MoreStrengthening customer relationships and making it easy to earn reward points is precisely what the Cat® Vantage Rewards program is designed to do.
Learn More