Cat® PM300 Cold Planer series
Cat® PM300 Cold Planer series

Design updates for next generation Cat® Medium Wheel Loaders improve operating efficiency and performance

 

For Worldwide Release: July 2024
Release Number: 155PR24

 

  • Refined technology features for all next generation Cat® 950 to 982 Wheel Loaders, including XE models
  • Auto differential lock improves operating ease
  • Available integrated tire pressure monitoring system shows on the machine display

First introduced with the Cat® 980 and 982 models, the next generation wheel loader design for Cat 950 to 982 models leveraged technology to usher in a new era of productivity, lower maintenance costs and increased fuel efficiencies. Caterpillar announces multiple technology refinements and performance updates on new machines to further increase efficiency and operating ease.

Excelling in performance

New auto front differential lock available for all 950 to 972 models with joystick steering and all 966 to 972 models with HMU (steering wheel) steering removes the burden from the operator by automatically engaging the differential lock to recover or maintain traction. Additionally, upgrades to both auto front and rear differential locks are options for the wheel loaders.

These medium wheel loaders feature improvements to the integrated brake system (IBS) and new engine RPM deceleration. The new transmission neutralizing features smooth engagement and disengagement with the IBS pedal.

Refined technology

The next generation wheel loaders introduced a range of technologies that helped operators to optimize machine use. Refinements and expansion of the wheel loader technology offerings help operators get more productivity out of the machines.

A new standard job-aid widget helps the operator in load-and-carry operations by automatically placing the bucket at the optimal height for stability and maximum material retention. Now linked to the work tool center, improvements to the zero-angle work tool widget enable the setting of different zero angles for different work tools and attachments.

Three programmable buttons on the implement control pod afford quicker access to regularly used functions to improve operating efficiency. Each operator can pull from over 25 different functions to customize and save their personal settings.

Key operating features – including Cat Payload, manual tip-off, neutralizer settings and tips, and application profiles – are now available in the on-board display system for quick reference and operator training. A new option for Cat Advanced Payload, e-Ticketing, can send the generated on-board weighing ticket as an electronic ticket to any preprogrammed email address within seconds of finishing the loading cycle, reducing paper ticket handling in the cab.  

For Cat 966 XE, 972 XE, 980 XE and 982 XE models, two new settings in application profiles allow each operator to set customized forward/reverse default speed ranges and rimpull limits. The speed and rimpull set limits are now visible to the operator on the front dash. Additionally, set site limits are shown on the operator settings screen, informing the operator of the established upper limit.

Improving reliability

Fully integrated in the machine’s systems, a new optional tire pressure measuring system shows the tire pressure on the main machine display, allowing operators to monitor tire pressure to improve performance, ride and reduce costs. Sensors transmit pressure information wirelessly to the system, and the desired target pressure can be adjusted based on tire type, manufacturer and model.

Cat Remote Flash and Remote Troubleshooting are standard features. Downloaded software update installations can now be initiated from the on-board display. Dealer remote troubleshooting functionalities have been expanded to include machine usage histograms and system calibrations. Preventative maintenance interval tracking can now be synchronized with VisionLink®, due-time reminders and overdue events are now shown to the operator on the display.

Operating convenience

Standard on premium cabs and optional for comfort and deluxe trim lines, a new left footrest improves operator comfort and provides effortless movements to the IBS pedal in powershift loader models and the deceleration pedal for XE models. Also, for all XE models, improvement to the speed range thumb roller adds a haptic detent for precise selection between 0.1 and 1.0 increments.

For 2- and 3-implement hydraulic functions, a new side grip implement joystick is now available on all joystick steering models to increase operator comfort. The improved optional active carbon cab prefilter design protects the operator environment from dust and particles. It also allows for easier retrofits and upgrades.

For more information about the latest updates for Cat Medium Wheel Loaders, contact a Cat dealer or visit: www.cat.com.

 

Download the press release and images 

Download Now

 

 

of

Cat PM310 Cold Planer

View Full Size Image
of

Cat PM312 Cold Planer

View Full Size Image
of

Cat PM312 Cold Planer

View Full Size Image
of

Cat PM312 Cold Planer

View Full Size Image
of

Cat PM313 Cold Planer

View Full Size Image

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

 

# # #

 

Note to Editors: Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, VisionLink, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.

©2024 Caterpillar All Rights Reserved

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Kate Kenny: Kenny_Kate@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Amy Doughty: Amy.Doughty@cat.com