“PRODUCTION EFFICIENCY IS WAY HIGHER BECAUSE YOU GET THE JOB DONE IN HALF THE TIME.”
An 861-acre site, five million cubic yards of earth to move and a tight timeline may sound daunting, but not to Brad Cole Construction.
“Having GPS technology allows us to be more competitive,” says Executive Vice President Ron Cryer of Cat Grade with 3D on the company’s dozers. “It’s really helped us on this project by allowing us to establish grades accurately and more efficiently.”
It’s helping Brad Cole Construction stay ahead of project deadlines, too.
“3D grade control definitely speeds up production,” says Project Superintendent Jeff Weaver. “It gives our operators the advantage of making one pass versus three or four passes.”
The result? “We’re actually slated to complete this project about 45 days early,” Cryer says. “That translates into a satisfied customer.”
Facing an enormous soil compaction challenge on an earthen dam project in northern Greece, the TENA SA crew tackled it with the help of Cat Compact.
TENA was responsible for placing 138 feet of compacted material on an existing 108-foot embankment, applying it in 7.8-inch layers and compacting it to 5.9 inches. Working in sandy clay made achieving uniform compaction and monitoring densities difficult.
Enter Machine Drive Power (MDP). This machine-integrated soil compaction measurement technology evaluates rolling resistance while it works, enabling much faster discovery of inconsistencies across an entire site—and it works in any type of soil.
“MDP saved us considerable time and certainly money,” says President and CEO George Nathanailidis—and he has the numbers to prove it. MDP helped eliminate a stunning 9,520 passes, and it more than doubled productivity on the remaining passes by increasing the compactor’s working speed from 1.2 mph to 2.8 mph.
“I would recommend others use it because of fast measurement compaction, accuracy, reliability and increased productivity,” Nathanailidis says.