If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For most of us, operating a machine means stepping inside the cab. Today, there are new options. Remote control technology could be the ticket to building a stronger safety culture and more efficient workforce. In this article, we explain how remote control technology could be key in keeping your crew safe and jobsite rolling.
Operating heavy equipment in a quarry is, simply put, not for the careless. Machine operators have to pay attention not only to their work and other equipment, but also to the site conditions around them. Failure to do so can have serious consequences.
A few sobering facts and statistics:
One of the less obvious hazards faced by quarry equipment operators is whole-body vibration. The constant stress of extreme vibration takes a toll, especially for dozer operators working on rocky terrain. Other equipment, such as front-end loaders and excavators, can induce jarring and jolting events that cause similar cumulative problems.
The bad news is whole-body vibration can lead to musculoskeletal disorders of the spine. It can also increase fatigue, which contributes to accidents in the short term, along with diminished motor performance capacity over the long run.
It’s a widespread problem that can lead to debilitating spinal issues. Between 2012 and 2016, surface mines and quarries reported a total of 523 non-fatal, days-lost injuries and no-days-lost injuries related to the back, neck and head.3
So, what can be done to limit injuries and accidents among quarry equipment operators?
But what if operators could do their jobs without working aboard their equipment at all?
With today’s remote-control technologies, operators can run dozers, excavators and wheel loaders from a safe, comfortable location away from their machines. They’re not subject to vibration or cab noise levels. And in some cases, multiple camera views — or simply a different viewpoint from off the machine — can provide enhanced visibility for more efficient operation.
To see what’s possible in remote control technology today, Command technology from Caterpillar is a good place to start.
Cat® Command was originally developed for mining applications, where the closed and controlled mine site environment offers fewer variables to contend with. The technology has now advanced to the point where it has proven viable for a wide range of quarry and construction applications.
Command technologies include two control configurations:
Of the two configurations, the Command Console system has the greatest impact on jobsite safety. For example, when a need arises to rescue a machine from a precarious location, the remote console allows operators to maintain line of sight to the machine but work out of harm’s way. They also require no on-site communications infrastructure. Operators could, for example, clean up a rock fall beneath a potentially unstable highwall without risk of personal injury.
Both systems retain smooth and precise machine control as if operating from the cab, and they offer complete access to advanced machine features. Built-in safety mechanisms shut down the machine in case of power or communications loss.
Command Stations can be located wherever the workforce may be. Operators don't have to commute to a distant or hazardous jobsite. In the future, they may even be able to work from home.
Both Command systems reduce the chances for jobsite and long-term injuries. Plus, they make recruiting and retaining operators much easier. Heavy equipment operation becomes something akin to playing a video game rather than hours on a moving seat. That’s an attractive advantage for a younger generation of potential operators.
In fact, remote control equipment makes good business sense at every level. Production can restart immediately after blasting. You get decreased downtime from faster shift changes and operator relocation. Best of all, you get a healthier, more productive crew that can work at top efficiency all shift long.
*****
1 https://mshau.com/the-5-most-common-mining-fatalities-probably-not-what-youd-think/
2 https://arlweb.msha.gov/Accinj/Accinj.htm
3 https://www.pitandquarry.com/preventing-exposure-to-whole-body-vibration/
You’re here to get ideas to grow your business. Read on for machine insights and expert tips and tricks to get more out of every job.
Keeping your operators safe on the job starts at the top. We discuss some ways to promote landscaper safety at your business.
Learn MoreKeep your snow and ice removal crew safe all winter long. We’re covering it all from injury prevention strategies, to personal protection equipment to routine machine maintenance. Plus, we’ve got you covered with Cat dealer training and e-learning resources.
Learn MoreLearn how contractors, aggregates producers and other equipment owners are using Cat® Technology to enhance safety and manage risk.
Learn MoreThe opioid epidemic is dominating a lot of headlines these days, with the Centers for Disease Control and Prevention reporting that opioids were involved in more than 42,000 overdose deaths in 2016 — five times that of 1999. But if you think that’s a problem for the D.C. bureaucrats to handle, think again.
Learn More