If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Excavating, lifting, loading and transporting materials: If your work requires any of these activities, then chances are you’ve got at least one loader on site. But is it the right type of loader for the task? Maybe you’ve only ever considered a wheel loader up to the job. Or maybe you’re loyal to the backhoe.
Here’s a quick refresher on the differences between these two types of loaders — and when it makes sense to choose one versus the other.
Wheel loaders offer high bucket capacities that make it fast and easy to load material onto trucks and move it across a site. They’re hands down the most efficient machines for lifting large quantities of practically anything — soil, gravel, rubble, debris, dirt, you name it.
That makes a wheel loader a smart choice for most material-handling jobs, whether that’s road building, site prep, logging, demolition or quarry work. You’ll also benefit from a wheel loader’s lifting capabilities if you need to clear a jobsite quickly or if you’re engaged in large-scale snow removal.
With attachments on both ends versus just the front, backhoes are versatile performers. Operators can use the articulated arm and small bucket on the back to dig, for example, then switch to the bucket on the front for material handling and leveling. Though backhoes typically don’t work as fast as wheel loaders, nor are they as maneuverable, they’re hard to beat when it comes to the range of tasks they can perform. Use a backhoe to:
Add attachments like grapples, hammers and stump grinders to expand use even further. A backhoe loader is a great option if your goal is to accomplish as much as possible with a single machine.
Once you’ve landed on the right type of loader for the task, make sure to choose the right weight and power combination for maximum efficiency. Here’s a general rule of thumb on loader size:
You’re here to get ideas to grow your business. Read on for machine insights and expert tips and tricks to get more out of every job.
Cat® Technologies gives you the accuracy, consistency and productivity you want.
Learn MoreThese words get used interchangeably, creating confusion. To improve consistency, we've defined these terms.
Learn MoreTechnologies that enhance machine performance can add to the bottom line.
Learn MoreAnswers on fuel efficiency from an expert - Jason Hurdis, GCI Global Market professional.
Learn More