If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Motor graders require more experience to run than any other machine, but thanks to Cat® Grade with cross slope, mastering this precision earthmoving machine is easier than ever.
Estimated read time: 3 minutes
Estimated watch time: 2 minutes
Setting up a precise grading profile with your Cat® motor grader is simple and easy thanks to the Grade with cross slope functionality built into the machine’s updated monitor. As you control one side of your blade manually, cross slope automatically adjusts the other side to accurately grade at your desired angle.
In this video you will learn about accessing the cross slope menu and settings.
CROSS SLOPE CONTROL NAVIGATION [00:16]
Your motor grader monitor is a command center that gives you, among other things, information on the position of the blade. Here’s how you begin using cross slope.
From the default menu screen, use the four-way soft key to select the cross slope information menu.
From there, press the right soft key button to display cross slope settings.
Here you can set valve speed, offset adjust and number of targets.
AUTO OR MANUAL [01:00]
Your motor grader always begins with blade control in manual mode. To use cross slope, you must put one side of the blade in automatic mode.
STEP-BY-STEP INSTRUCTIONS TO USE CROSS SLOPE
Disengage the parking brake.
Make sure that there is no articulation, the circle is centered and there is no wheel lean.
Ensure that the implements are not locked out.
Check there are no active diagnostics on a required input or output.
Raise the blade off the ground.
Set/change target slope value.
Place the desired side in auto mode.
Use the joystick on the manual side to control the height of the blade.
Modify your presets (favorites) so you can access those with the click of a button.
LOCK IN YOUR TARGET SLOPE
The cross slope information menu contains several ways to adjust the position the blade. Once you enter numerical values, they will appear on the monitor screen. You can:
Set increment/decrement with the thumb rollers.
Bench the blade on a desired slope and then push both thumb rollers up simultaneously to match the blade position to the slope.
Preset the target using the yellow button on the right-hand roller.
Swap target direction for turnarounds by pushing both rollers down at the same time.
CROSS SLOPE INDICATE SYSTEM
If equipped, the cross slope Indicate system provides precise cross slope and mainfall feedback. Change the position of the blade with the joysticks, and those values will change automatically on the monitor. Cross slope indicate can be upgraded to automatic cross slope. Just contact your Cat dealer for more information.
Have any questions about using features on your motor grader monitor after watching this video? Check your Operation and Maintenance Manual or contact your Cat dealer.
Get the most from your motor grader with operating tips, safety advice, maintenance help and much more.
Boost visibility from your cab with Cat Detect with Smart Camera.
SEE THE DIFFERENCEDon’t get intimidated: Learn motor grader lever controls and work confidently.
START GRADING NOWThis Cat® parts and service app provides a world of expertise.
SEE MOREIn this video, see how to become a Cat® Grade with 3D pro.
WATCH NOWGain unlimited access to must-know information about your machine. Find ideas you can put to work on the job right away, including business insights.