If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
If you already have an existing account with another Cat App, you can use the same account to sign in here.
Account Information
Site Settings
Security Settings
GTUIT SOLUTION PROCESSES UP TO 100% OF FLARE
Gas typically gets flared because it’s problematic — there’s too much variation in its chemistry, flow rates, pressures and temperatures for it to be usable without requiring a lot of costly treatment. But what if you could solve those problems on your site in an economical way, put the cleaned-up gas to good use and make a dent in your ESG (environmental, social, governance) goals all at the same time? That’s what GTUIT makes possible.
GTUIT, a company in which Caterpillar holds an equity investment, is the industry leader in field and well-site natural gas processing and conditioning. The company’s proprietary mobile solution enables energy companies to process up 100% of flare volumes, remove up to 80% of C3+ hydrocarbons and significantly reduce emissions, all while turning flare gas into additional revenue and increasing the potential for oil production.
In 2019, GTUIT’s solutions helped its customers eliminate almost 557,000 tons of CO2 through the production of natural gas liquids (NGLs) from flare gas.
Lower cost, smaller footprint, quicker setup
Traditionally, oil and gas operations must invest in separate dehydration, compression and refrigeration equipment on site to treat flare gas. It can be expensive to acquire and maintain, plus it’s not mobile and requires permitting. GTUIT’s solution, on the other hand, integrates all that equipment onto a single trailer — one that can be moved on or off location in a matter of hours — reducing the gas treatment footprint on site and requiring no permits. Daily site checks, equipment setup, troubleshooting, maintenance, spare parts and repairs all are included in one fee.
Making unusable gas usable — and profitable
The GTUIT solution produces conditioned dry gas and achieves maximum NGL recovery — dramatically reducing emissions and conserving energy for later use. The resulting gas and NGLs can be used across a number of different applications on fracking, drilling, gas compression and production sites, such as:
The GTUIT solution is applicable anywhere in the world gas is flared — or anywhere associated gas needs effective, inexpensive treatment. Want to learn more about how it can help you meet your environmental and economic goals ? Get details at www.gtuit.com or talk to your local Cat dealer.
Finding a solution that delivers both environmental and economic benefits has been tricky — until now. The Cat® 3512E Tier 4 Final DGB™ Engine strikes the right balance for frac operations.
Learn MoreWith proponents of electric fracking claiming cost savings of $1 million a month, it’s easy to get caught up in the hype. But take a careful look at the numbers to see if those savings are a reality for your operation.
Learn MorePairing gas generators with batteries, the Cat® Land Drilling Energy Storage System not only reduces emissions and fuel use significantly but also improves power quality and transient response.
Learn MoreOnly one product delivers performance that’s the same as when new at a fraction of the cost — plus material, water and GHG savings. Find out why Cat® Reman is the smart choice for oil and gas operations.
Learn More