Get the job done comfortably and safely when you're working in the cold.
By Caterpillar | Updated: February 2024
Hard work doesn’t stop just because it’s cold outside. We’ve put together tips so you can get your job done comfortably and safely, even during the cold winter.
Multiple lighter layers are better than one thick layer. Why? Because the air warmed by your body heat gets trapped between each layer. More layers = more warm air keeping you comfortable. Each layer serves a different purpose:
It’s a myth that you lose half your body heat from your head (it’s more like 10%). But it’s still important to keep your head and neck covered. Wear an insulated face mask, neck covering and a hat, or consider a balaclava.
Keep your hands warm while still being able to do precise, detailed work with a pair of water-resistant gloves like these that are padded and lined for warmth.
Wear two pairs of socks. The first pair is a base layer that wicks away moisture and keeps your feet dry. The second pair should be a wool-like material that provides a thick layer of insulation and keeps your feet warm. Our collection of Cat socks are made from breathable, moisture wicking material that stretches.
Consider composite toe boots instead of steel toes – they don’t conduct cold and will keep your feet warmer. Slip-resistant boots, like the ones shown here, help provide extra grip and prevent falls while walking on slippery wet ice.
Shoes or boots should be both fully insulated and waterproof. Consider going up a shoe size to ensure room for both layers of socks and room to move your toes.
You can always be prepared. Socks get wet. Gloves and hats go missing. Be equipped with extras.
As your body tries to stay warm, it will burn extra calories. Make sure you eat enough at mealtimes and, if needed, plan for snacks.
You know it’s important to hydrate in the heat. But it’s also crucial in the cold — dry winter air causes you to lose a considerable amount of water, especially when working hard. Avoid beverages that contain alcohol or caffeine – they’re dehydrating. Keep water with you in a thermos like this one to prevent it from freezing.
Your friends and family who work in the trades know the value of quality and durability — and that’s exactly what these gifts for construction workers, contractors and builders deliver. Give the perfect gift from our Gifts for Construction Workers guide.
Shop Now MerchandiseEquipment downtime can delay your projects. Read about the top ways to prevent downtime, including the use of equipment monitoring and proper storage steps.
Learn MoreHeavy equipment gets dirty. Knowing how to clean heavy equipment properly, including tips on pressure-washing for heavy equipment, will keep machines in top shape.
Learn How Equipment MaintenanceKenny Nichols, long-time dozer operator and Cat equipment owner, has dedicated his life to doing the work he loves. With 84 years and 110,000 hours behind the controls, he may be the most experienced dozer operator around.
Learn More