Engineering Innovation

Lemgo
Lemgo

Cat® Dealer Provides Customized Engineering Solutions to Optimize Cogeneration

Customer:  Stadtwerke Lemgo

Location:  Lemgo, Germany

Customer Business Issue:  The need for decarbonization of power generation and district heating capabilities driven by local regulations and community initiatives

Solution: Innovative combined heat and power (CHP) technologies customized through local engineering expertise

Cat® Dealer:  Zeppelin Power Systems

 

POWER NEED

Located in the Lippe district of Germany’s North Rhine-Westphalia, the town of Lemgo has a rich history dating back nearly 850 years. It is the home of Technische Hochschule Ostwestfalen-Lippe, a research university that specializes in the applied sciences, focusing on mechanical engineering and industrial electronics. Lemgo is also renowned for its half-timbered architecture dating back to the Renaissance, including the Hexenbürgermeisterhaus finished in 1571.

Stadtwerke Lemgo, the local municipal utility, provides electric power and district heating for the town, currently supplying approximately 160 million kilowatt-hours of heat annually. 

Stadtwerke Lemgo is committed to reducing its environmental impact by supporting the goals of the 3rd Lemgoer Klimaschutzkonzept, a climate protection initiative aiming to reduce carbon emissions in the town by 90% from 1990 to 2050. 

Over its extended relationship with Stadtwerke Lemgo, Zeppelin Power Systems, the local Cat® dealer, has served a major role in helping the utility meet its goals by supplying engineering, installation, and service expertise for nine Cat natural gas-fueled combined heat and power (CHP) systems that currently supply a total electrical output of 18 MW.

Most notably, Zeppelin supplied Stadtwerke Lemgo’s CHP units in 2021 as part of an integrated system that was named “CHP of the Year 2022” by Germany’s Federal Association of Combined Heat and Power and Energie & Management magazine.

SOLUTION

The solution combines a 7.5 MW CHP system powered by three Cat G3520 natural-gas generator sets, a 5.2 MW solar thermal system with vacuum tube collectors, and a heat pump that generates up to 1 MW of thermal output using water from the Bega River. With the addition of these new thermal capabilities of solar thermal and a heat pump, up to 20% of district heating produced by Stadwerke Lemgo is currently generated carbon-free.

This award-winning system is the latest in a series of innovations supported by the team at Zeppelin. A previous milestone was achieved in 2019, when engineers from Zeppelin updated a CHP system powered by an existing Cat G3516H generator set with a state-of-the-art ammonia heat pump that recovers heat from the second-stage intercooler and exhaust heat condenser. Zeppelin also installed a second heat pump configured to recover heat from treated sewage plant discharge water. Combined, the two new heat pumps deliver over 3.3 MW of hot water for district heating which represents two-thirds of the historic city center heat needs.

Zeppelin designed and managed the modification of the CHP system, which included the delivery of the heat pumps and required control systems, switchgear, and ventilation. Additionally, Zeppelin provides ongoing support through long-term service agreements, which include regular maintenance at scheduled intervals as well as around-the-clock, on-demand technical assistance.

RESULTS 

Facilities can reduce operating costs by implementing a Cat CHP system or a combined cooling, heat, and power (CCHP) system. Most Cat natural gas-fueled engines can be configured with a CHP or CCHP system to simultaneously generate power for electrical loads while capturing waste heat that can be repurposed as thermal energy for facility processes or heating, ventilation, and air conditioning (HVAC) requirements.

While the combination of grid power and traditional boilers for thermal energy offers less than 50% energy efficiency, CHP and CCHP systems from Caterpillar can provide total energy efficiencies of up to 90%. This allows customers to save on energy spending, provide autonomy of supply, and reduce emissions.

Cat CHP and CCHP systems can deliver a rapid return on investment for a wide range of industrial and commercial facilities, such as manufacturing plants, refineries, regional district heating plants, resorts, shopping malls, high-rise office buildings, universities, data centers, and hospitals.

Download the Power Profile

Featured products

  • COMBINED HEAT AND POWER

    Cat® Combined Heat and Power (CHP) systems can lower operating costs and emissions. Ask a Cat dealer how Cat cogen systems can increase efficiency up to 90%.

    Learn More
  • Gas Standby Rating
    2500 ekW @ 0.8pf
    2500 ekW @ 0.8pf
    Fuel Type
    Natural Gas, Hydrogen Blend (up to 5%)
    Natural Gas, Hydrogen Blend (up to 5%)
    Emissions/Fuel Strategy
    U.S. EPA Stationary Non-Emergency Certified
    U.S. EPA Stationary Non-Emergency Certified

    G3520 with FAST RESPONSE

    Caterpillar is leading the power generation marketplace with Fast Response generator sets engineered to deliver unmatched performance, reliability, and cost-effectiveness.

    Learn More
  • Gas Standby Rating
    2000 ekW @ 0.8pf
    2000 ekW @ 0.8pf
    Fuel Type
    Natural Gas, Hydrogen Blend (up to 5%)
    Natural Gas, Hydrogen Blend (up to 5%)
    Emissions/Fuel Strategy
    U.S. EPA Stationary Non-Emergency Certified
    U.S. EPA Stationary Non-Emergency Certified

    G3520 with FAST RESPONSE

    Caterpillar is leading the power generation marketplace with Fast Response generator sets engineered to deliver unmatched performance, reliability, and cost-effectiveness.

    Learn More

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products
electric power
electric power

Generator Set Sizing Calculators

Caterpillar Electric Power now has two tools available for sizing gensets in any application. 

Size Now
genset sizing
genset sizing

Utilities

You supply power to meet everyday needs, whether it’s lights in a school, appliances in a home, or keeping an office building in business. It’s why you need a source that promises to run non-stop — since life does, too.

View Utilities Page
Utilities
Utilities

CAT DEALERS MAKE THE DIFFERENCE

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service and support.

CONNECT WITH YOUR DEALER TODAY
dealers
dealers