PLUG AND PLAY EASE 

Plug and Play Electronic Cat® C4.4 Gen Set Provides Power and Reliability to Support Mississippi River Mat Work

H&H Marine - Case Study
H&H MARINE REPOWERS U.S. ARMY CORPS OF ENGINEERS' TOWBOAT

The U.S. Army Corps of Engineers (USACE) leverages its engineering expertise to promote stability and improve quality of life. It provides public engineering services to strengthen national security, energize America’s economy, and reduce infrastructure risks from hurricane and storm damage.

Case Study

CUSTOMER:

H&H Marine Services

DEALER:

Puckett Power Systems

SEGMENT:

Inland Waterway

SOLUTION:

Repowers

LOCATION:

Mississippi, USA

SCOPE OF ENGINE USE:

Cat® C4.4 (Electronic)

In Mississippi, the USACE’s Mat Sinking Unit (MSU) places hundreds of thousands of articulated concrete mats, also known as revetment, along the Mississippi River to protect flood control works, prevent riverbank erosion and provide navigable waterways for commercial transportation. The unit’s work spans the Memphis, Vicksburg and New Orleans districts’ jurisdictions and more than 1,700 river miles. Normally, 4x25-foot sections of mat are tied together to make a square, and 35 squares form a launch. Each supply barge holds 585 squares of mat, consisting of 950 tons of concrete.
The main job for the towboat M/V Harrison is pushing mat for the MSU. Built in 1986, the vessel’s Cat® 3304 generators had been overhauled twice. As the engines had accumulated 90,000 hours of service, USACE sought to give the 1,200-horsepower towboat a new lease on life.

Dockside Turnkey Repower Saves Time and Costs

USACE turned to Vicksburg, Mississippi-based H&H Marine Services for assistance with the project. Having performed the M/V Harrison’s previous overhauls, H&H Marine was familiar with the towboat and understood the technical requirements needed to enable the vessel to perform the intense mat work.

A pair of Cat C4.4 engines was recommended for the gen set repower for several reasons. With its newly redesigned cooling system, the Cat C4.4 allows a repower to be performed dockside rather than at a shipyard, saving considerable time and cost. As a standardized plug and play package, the Cat C4.4 ensures parts availability for the life of the engine while delivering the robust, reliable performance USACE had experienced with its previous Cat engine. Additionally, Cat dealers are no more than 75 miles from anywhere on the Mississippi River, ensuring quick and easy access to skilled service and support when needed.

Responsive, Skilled Support

Having performed 20 repowers over the past 10 years, H&H Marine turned to Cat Dealer Puckett Power Systems to facilitate the dockside project. Puckett has provided H&H Marine dependable and responsive support for 20 years, supplying parts, drawings and technical expertise for every type of project. 

Puckett provided the fittings, hoses and other components to make the generator drop-in ready. Only a day was needed to remove the Cat 3304 generators. The compact, self-contained design of the Cat C4.4 engine enabled H&H Marine to use the existing skid, saving the time and expense of having to cut the skid from the boat. The new gen set matched all the existing plumbing and electricals, speeding the installation process. Additionally, the newly redesigned cooling system not only reduced project cost but also eliminated the need to install new piping; important for older boats’ limited room.

With the installation complete, Puckett performed the startup and commissioning services. The entire project took just 10 working days – much faster than shipyard repowers.

Plug and Play Ease

The m.v. Harrison is currently in operation, and the USACE is pleased with the quick return to service and performance of the towboat’s electrical service. Based on the long life of the current gen set’s predecessor, the organization looks forward to many hours of use which helps lower total cost of ownership (TCO).

“The Cat C4.4 packs a lot of power in a drop-in package, providing the reliability and serviceability workboat operators need,” said Paul Henson, owner of H&H Marine Services. “Working with Puckett Power Systems enables us to perform dockside repowers quickly and cost-effectively.”

Gary Sarrat Jr., Caterpillar Marine inland & tug segment key account manager added, "The trim design and single circuit cooling system allow the electronic Cat C4.4 engine to be a turnkey gen set solution that keeps repower costs low and meets today’s towboat operators’ needs.”

 

 


WANT TO READ MORE CASE STUDIES?

Read more Marine Case Studies and discover how Caterpillar Marine can help you succeed.

Check Out Our Other Articles
See more Marine Case Studies

Marine Power Solutions Guide

With the Marine Power Solutions Guide, compare engines, specs and aftertreatment systems and find the right system for your marine operation.

Download Now
Marine Power Solutions Guide

Connect With Your Dealer

Talk with product and solution experts to see how Caterpillar can work for you.

Connect With Dealer
Connect With Your Dealer

STAY CONNECTED TO MARINE WITH ADDITIONAL INFORMATION

MARINE BLOG

Dive into the Cat® Marine Blog Beyond the Iron and explore posts about innovative products and solutions, industry trends, maintenance tips, upcoming trade shows, and more.

Read Now
Cat Marine Blog

Marine Case Studies

Read one of the case studies below to learn first-hand from our customers why they choose Cat® Marine to power their operations when they are out on the water.

Learn More
Marine Case Studies

MARINE PODCAST

Tune in to the Cat® Marine podcast for straight talk and expert insights on what’s working, what’s new and what’s trending in the global marine industry.

Tune In Now
Cat Marine Podcast

Marine News

Stay current on the latest Marine engine stories and announcements.

See What's New
Marine News