Matching the performance of the diesel-powered R1700 and using switch reluctance (SR) technology, the R1700 XE features fast-onboard charging, allowing the batteries to be charged while remaining on the machine.
TUCSON, Ariz., September 21, 2024 – The electric Cat® R1700 XE Load Haul Dump (LHD) displayed at MINExpo 2024 offers 100% battery-electric propulsion, producing zero exhaust emissions and significantly less heat generation than a reciprocating engine powered model. Matching the performance of the diesel-powered R1700 and using switch reluctance (SR) technology, the R1700 XE features fast-onboard charging, allowing the batteries to be charged while remaining on the machine. The Cat MEC500 Mobile Equipment Charger fully charges the R1700 XE in less than 30 minutes with a single charger and less than 20 minutes using two units.
# # #
Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.
Caterpillar Inc. is launching its next generation of Cat® Telehandlers. Released for retail and rental customers, the Cat TH0642, TH0842, TH1055 and TH1255 models replace the previous TL642, TL943, TL1055 and TL1255 machines.
Learn MoreCaterpillar Inc. is announcing the new Cat® D8 dozer with advanced technology designed to provide faster more accurate results.
Learn MoreCaterpillar Inc. will launch its Centennial Celebration during CES 2025, providing visitors the opportunity to reflect on the company’s global impact over the last century and envision what’s in store for the future.
Learn MoreCaterpillar is announcing Cat® Command for Loading is expanding to all medium wheel loaders, excluding the GC models.
Learn More