The Cat® 995 Wheel Loader features a higher rated payload and 6% increase in hydraulic force with equal cycle time to deliver up to 19% increased productivity compared to the 994K.
TUCSON, Ariz., September 21, 2024 – The Cat® 995 Wheel Loader is built to the same size as the 994K it replaces. Yet, it features a higher rated payload and 6% increase in hydraulic force with equal cycle time to deliver up to 19% increased productivity. The higher payload rating enables a one-pass reduction when loading Cat 785, 789 and 793 Mining Trucks, equaling up to a 33% increase in production and efficiency when loading the 785, up to a 25% increase with the 789 and up to a 20% increase with the 793.
o Up to 11% lower hourly fuel consumption and up to 30% efficiency gain when operating in Enhanced Eco Mode compared to throttle lock mode on the 994K
o Redesigned, pressurized next generation cab offers 50% more legroom, reduced vibration feedback, lower sound levels and automatic temperature control
o Taller windshield provides a 25% increase in glass surface area and a 64% increase in wiper sweep area improves visibility to the bucket
o Tip up prevention technology avoids unnecessary stress on drivetrain and structures
o Optional Autodig components automates three of the dig cycle’s most difficult parts:
o Optional Operator Coaching measures and reports on individual operator behaviors that impact efficiency, production and component life
o Optional Payload Overload Prevention allows a larger bucket to be used to achieve pass-match targets without the risk of overload
o All service areas are accessed from either ground level or a platform, improving safety
o 500-hour engine oil change interval and improved air filter life
o Number of steering hoses has been reduced from 15 to 10 and tubes cut from 11 to 1, along with elimination of neutralizer adjustment, to improve serviceability
# # #
Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.
Caterpillar Inc. is launching its next generation of Cat® Telehandlers. Released for retail and rental customers, the Cat TH0642, TH0842, TH1055 and TH1255 models replace the previous TL642, TL943, TL1055 and TL1255 machines.
Learn MoreCaterpillar Inc. is announcing the new Cat® D8 dozer with advanced technology designed to provide faster more accurate results.
Learn MoreCaterpillar Inc. will launch its Centennial Celebration during CES 2025, providing visitors the opportunity to reflect on the company’s global impact over the last century and envision what’s in store for the future.
Learn MoreCaterpillar is announcing Cat® Command for Loading is expanding to all medium wheel loaders, excluding the GC models.
Learn More