This product specific system forms part of Caterpillar’s comprehensive training program for the Cat 798 AC truck and features a direct replica of 798 AC operator controls, complete with a six-degree-of-motion platform.
TUCSON, Ariz., September 21, 2024 – Cat® Equipment Training Solutions will introduce the Cat 798 AC driver training simulator, developed by ThoroughTec Simulation, at MINExpo 2024. This product specific system forms part of Caterpillar’s comprehensive training program for the Cat 798 AC truck and features a direct replica of 798 AC operator controls, complete with a six-degree-of-motion platform. The simulator is designed to effectively train operators in the most efficient, safe and realistic way possible, including an ultrahigh definition replication of the mining environment in which the truck operates. The system also comes complete with dual screens at the instructor’s desk with the ability to provide a flyover view of the entire mining operation as well as monitor equipment and exercise parameters.
More information available www.catoperatortraining.com.
# # #
Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.
Caterpillar Inc. is launching its next generation of Cat® Telehandlers. Released for retail and rental customers, the Cat TH0642, TH0842, TH1055 and TH1255 models replace the previous TL642, TL943, TL1055 and TL1255 machines.
Learn MoreCaterpillar Inc. is announcing the new Cat® D8 dozer with advanced technology designed to provide faster more accurate results.
Learn MoreCaterpillar Inc. will launch its Centennial Celebration during CES 2025, providing visitors the opportunity to reflect on the company’s global impact over the last century and envision what’s in store for the future.
Learn MoreCaterpillar is announcing Cat® Command for Loading is expanding to all medium wheel loaders, excluding the GC models.
Learn More