If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
When it’s time to rebuild, repair or purchase a replacement on-highway truck engine, consider Cat® Reman. Cat Reman engines are remanufactured to like new condition. And owners and operators of Cat Reman engines gain access to valuable Cat service and support through our network of authorized Cat dealers.
Estimated read time: 4 minutes
Hard-working Cat® engines are found under the hoods of more than 1 million on-highway trucks across North America, powering medium- to heavy-duty applications.
And while Cat engines are built to last, they'll eventually need a repair, rebuild or replacement. That's where Caterpillar's line of remanufactured truck engines comes in. Supported by a range of replacement parts and kits, Cat Reman engines are designed to provide like new quality for additional lifecycles.
What if your Cat engine is due for an overhaul? A Cat Reman engine is a drop-in solution, meaning it comes fully assembled and quality-tested for your truck. Watch this video for more details:
[NEW VIDEO WHEN AVAILABLE]
The Cat Reman process begins when you return used engine components — known as core — to your authorized Cat dealer. They’ll inspect it and issue a core refund, which you can use as credit toward your purchase of a Cat Reman complete engine.1
Once the dealer inspects and approves the core, it goes through an intensive remanufacturing and salvage process at one of Caterpillar’s remanufacturing facilities. There, components are disassembled down to individual piece parts, cleaned and inspected.
Then, they’re remanufactured to Caterpillar performance specifications with all the latest engineering updates. Ultimately, Cat Reman engines offer like new performance and, with core return, they’re available to customers for a fraction of the price of new with core return.1
Your authorized Cat dealer can help you decide if you need repairs, a rebuild or a full replacement. Incorporating fully assembled Cat Reman engines can shorten your repair time and, when you return core1 can even save you money. The good news is that Cat Reman has an engine option for many on-highway applications.
Some of the components you may be able to secure for an engine repair or rebuild include precious metals kits [link to PMK article when it is published], air compressors, cylinder packs, injectors, oil pumps, turbochargers … and the list doesn’t end there.
Medium-duty Cat Reman engines [link to OHTE-23-002] — C7, 3116, 3126, 3126B/3126E — are backed by a same-as-new Caterpillar Limited Warranty2. They come fully assembled with the air compressor, flywheel, main engine wiring harness, electronic control module and all engine sensors for a fast, efficient overhaul.
If you’re running heavy-duty applications — Cat C-10, C-12, C13 ACERT, C-15, C15 ACERT and 3406 engines — you have several options.
Complete Cat Reman engines, which are fully assembled for a fast, efficient overhaul. The electronic control module (ECM), engine wiring harness and sensor set and complete set of oil and fuel lines are included — and backed by a 24-month Caterpillar Limited Warranty2.
Complete Cat Reman engines with new content, which come with new cylinder blocks, crankshafts and cylinder heads, so you can upgrade to a new model or repower your truck from another engine brand. Plus, you’ll get our 24-month Caterpillar Limited Warranty.2
In addition to complete Cat Reman engines, you can also find Cat Reman long blocks, Cat Reman long blocks with new content and Cat Reman short blocks. All options are backed by a same-as-new Caterpillar Limited Warranty2.
So how can you get the process started? First, connect with your authorized Cat dealer to select which repair option is right for you. Here are just a couple you could consider:
Option one: Cat Reman engines, which are disassembled, cleaned, inspected, salvaged and remanufactured to Caterpillar performance specifications with the latest engineering updates. Then, they’re tested to ensure they deliver like new performance. Choose Cat Reman if your existing core is still in good condition. That way, you get the quality you want at a cost-effective price.
Option two: Cat Reman engines with new content, which give you the chance to repower your truck without starting from scratch. They contain 100% new cylinder blocks, crankshafts and cylinder heads. This gives you maximum life expectancy, enhanced overhaul potential and peace of mind. With this option, you don’t need to worry if your core is damaged as we accept most cores, even rusted and corroded ones. It’s like resetting your engine and giving the heart of your truck a jump-start.
So, if it’s time to overhaul your on-highway truck engine, talk about Cat Reman products with your local authorized Cat dealer. They’ll help you spec a Cat Reman engine or long block.
Check out Cat Reman engines and blocks to find the right on-highway engine for your application today.
1Cost savings based on return of core; core conditions apply.
2Warranty can vary by model and application; limitations may apply. For complete details about the applicable Caterpillar Limited Warranty, contact an authorized Cat dealer.
Get the most from your on-highway truck engine with information about repair options and more.
Alan Kitzhaber's Cat® 3406E engine has taken him on a four-million-mile journey. Learn the secrets to his trucking success.
Hear Alan's StoryThis 56-year trucking veteran has put three million miles on his Cat® truck engine and driven more than 6.5 million overall.
Meet DaleFrom a single part to a complete remanufactured engine, here's how we keep you rolling.
Learn More