Higher Power

heber
heber

Cat® Gas Generator sets Power High Altitude Utility in Extreme Conditions

 

Customer: Heber Light & Power 

Location: Heber City, Utah

Customer Improvement: Working with Caterpillar in field-follow studies to show that gas gensets save businesses money when grid prices are over gas prices.

Customer-owned Utility Products: Cat gensets: two G3516C, three G3520C, two G3516A, one G3516H, one G3520H, one G3520

Cat® Dealer: Wheeler Power Systems

 

of

Their latest generator set is the G3520, which is the first ever US EPA Certified natural gas generator set at 2 and 2.5 MW power output.

of

For many years, Heber has strategically partnered with Caterpillar by testing their electric power equipment during field follow studies before the generator sets become available for purchase in the marketplace.

of

Heber Light & Power has been running this generator on their site for the past year during its field follow study.

of

Heber Light & Power operates nine gas generator sets, each ranging from 750 kW to 2.0 MW of electrical output. In early May of 2015, the utility added the first ever Cat® G3512H generator set.

of

Heber City, Midway City, and Charleston Town – the co-owners of the utility – as well as customers in Daniel, Independence, and Wasatch counties are located 45 minutes from downtown Salt Lake City at an elevation of 5,600 feet (1,707 meters).

of

In the summer, when local demand peaks at 37 MW and the cost of purchasing energy is expensive, Heber Light & Power may strike all nine generator sets. During the spring and fall when demand is lower, days can go by when all the generator sets are quiet.

of

“These generator sets help us manage our resources and keep the cost of power down,” said Alan McDonald, chairman of the board for Heber Light & Power. “With this option, we don’t find ourselves having to buy electricity at top dollar during the high peak demand time.”

of

“We are proud of our track record in working directly with Heber Light & Power to show them how they can effectively maintain their equipment and keep their customers’ rates down,” added Josh Kinsey, product support representative for Wheeler Machinery.

of

The reliability and ready availability of the Cat® generator sets will enable Heber Light & Power to add sustainable sources of energy, including renewables, to the utility’s mix of power sources on an accelerated timetable.

POWER NEED

Heber Light & Power, a customer-owned utility based in Heber City, Utah is a long-time Caterpillar Electric Power customer with a variety of Cat  generator sets including two G3516C, three G3520C, two G3516A, one G3516H, and one G3520H with a total capacity of 13MW. Heber Light & Power is an inter-local government entity owned by Heber, Midway, and Charleston, Utah. They have a defined service territory in Wasatch County Utah powering about 12,000 end-use customers.

For many years, Heber has strategically partnered with Caterpillar by testing their electric power equipment during fieldfollow studies before the gensets become available for purchase in the marketplace. “The purpose of field-follow studies are to accumulate endurance hours on our equipment to ensure performance is meeting our stringent standards before making products available for purchase,” said Shane Minor, utility, governmental, international sales representative at Wheeler Power Systems, Heber’s local Cat dealer.

Because the large-scale standby electric power industry has seen a turn toward natural gas gensets, Caterpillar Energy Solutions has been researching and developing new solutions in this space. Their latest genset is the G3520, which is the first ever U.S. EPA Certified natural gas generator set at 2 and 2.5 MW power output. Heber Light & Power has been running this generator on their site for the past year during its field-follow study.

SOLUTION

“We’ve tested many units for Caterpillar and work closely with their engineering group,” said Jason Norlen, general manager of Heber Light & Power. The G3520 was installed last year, and since then we’ve run over 5,000 hours on it. It’s running extremely well at 2.5 MW at 1 g/bhp-hr NOx emissions. One of the benefits of our arrangement with Caterpillar is getting to see innovative new products like this one before they’re even on the market. I’ve never seen a gas unit perform like this one. It’s torquey like a diesel, and it’s very comparable to a diesel unit with how fast it responds and takes load on.”

“The Heber utility is located at 5,600 feet altitude,” said Norlen. “This altitude level would normally take a natural gas engine and knock its performance in the dirt, but this G3520 has pulled 2.5 MW from the moment it came in – which is impressive.”

“One of the huge benefits of testing gas generators at the Heber location is subjecting them to some extreme conditions during the field follow,” said Minor. “The units ran at 103  F temperatures in the summer and at 10  F in the winter at various humidity levels, and the performance of this generator set has not been impacted. It also runs in the same engine room as other units. When heat radiates from other units, it can create a more challenging environment, but that has not been an issue with this unit either.”

While field-follow hours for this unit were performed at a utility site, it’s ideal for emergency, legally required, or optional standby systems, as it was designed with quick-start enabling technologies and starts in 7.5 seconds The G3520 is suitable for office buildings, data centers, retail complexes, schools, government buildings, universities, and research as well as industrial facilities.

With an updated package design, the G3520 is modeled after the standby diesel solution to minimize installation costs and commissioning time on-site. A high-power-density 20-cylinder engine offers market-leading load acceptance and transient response. “This generator was designed for reliability,” said Minor. “It’s built upon a robust diesel 3500 platform with a proven track record, which is critical for our customers who use these generators during utility outages.”

RESULTS

Heber Light & Power uses Cat gas generator sets to offset high utility costs as they fluctuate. When deployed for peaking support and other strategic purposes, gas generator sets deliver high efficiency, increase the diversity of the power generating portfolio, protect power quality, and shield against market power price volatility. These factors help utilities like Heber Light & Power improve their financial position, differentiate their service to customers, and support community economic growth.

“We’re constantly evaluating the cost of electricity from the grid versus the cost of natural gas,” states Norlen. “We evaluate whether or not to run the gas engines daily, when the cost of natural gas is lower than electricity from the grid, we run the gas engines. Using the gas generator sets when the cost of power increases drives down overall wholesale power cost for the utility, it’s such a small piece of the portfolio, but it’s the top-end piece.” On average Heber saves several hundred thousand dollars a year when power prices are higher than gas prices.

Caterpillar is a leader in the power generation industry with market leading power systems engineered to deliver unmatched flexibility, expandability, reliability, and cost-effectiveness. With parts and service available globally, Caterpillar offers worldwide product support through its comprehensive service and dealer network, where technicians are trained to service every aspect of the equipment.

Download the Power Profile

 

Featured products

  • G3516A
    Continuous Rating
    1085 ekW
    1085 ekW
    Fuel Type
    Natural Gas, Biogas, Coal Gas
    Natural Gas, Biogas, Coal Gas
    Maximum Electrical Efficiency
    36.50%
    36.50%

    G3516A

    From natural gas-fueled combined heat and power (CHP) systems and emergency power for facilities, to renewable biogas energy to support the local grid, or electricity generated from coal mine gases, Caterpillar has a wide range of reliable gas power solutions.

    Learn More
  • G3516C
    Continuous Rating
    1660 ekW
    1660 ekW
    Fuel Type
    Natural Gas
    Natural Gas
    Maximum Electrical Efficiency
    37.70%
    37.70%

    G3516C

    From natural gas-fueled combined heat and power (CHP) systems and emergency power for facilities, to renewable biogas energy to support the local grid, or electricity generated from coal mine gases, Caterpillar has a wide range of reliable gas power solutions.

    Learn More
  • G3516H
    Continuous Rating
    2027 / 2007 ekW @ 1.0pf
    2027 / 2007 ekW @ 1.0pf
    Fuel Type
    Natural Gas, Hydrogen Blend (up to 25%)
    Natural Gas, Hydrogen Blend (up to 25%)
    Maximum Electrical Efficiency
    45.30%
    45.30%

    G3516H

    From natural gas to biogas, coal mine gases, or hydrogen fuel blends to support combined heat and power (CHP), emergency power, and local grid support applications, Caterpillar has a wide range of reliable gas power solutions.

    Learn More
  • G3520H
    Continuous Rating
    2519 / 2500 ekW @ 1.0pf
    2519 / 2500 ekW @ 1.0pf
    Fuel Type
    Natural Gas, Hydrogen Blend (up to 25%)
    Natural Gas, Hydrogen Blend (up to 25%)
    Maximum Electrical Efficiency
    45.30%
    45.30%

    G3520H

    From natural gas to biogas, coal mine gases, or hydrogen fuel blends to support combined heat and power (CHP), emergency power, and local grid support applications, Caterpillar has a wide range of reliable gas power solutions.

    Learn More

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products
electric power
electric power

Generator Set Sizing Calculators

Caterpillar Electric Power now has two tools available for sizing gensets in any application. 

Size Now
specsizer
specsizer

Utilities

You supply power to meet everyday needs, whether it’s lights in a school, appliances in a home, or keeping an office building in business. It’s why you need a source that promises to run non-stop — since life does, too.

View Utilities Page
Utilities
Utilities

CAT® DEALERS MAKE THE DIFFERENCE

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service and support.

CONNECT WITH YOUR DEALER TODAY
dealers
dealers